Product profile
Hydrosart® shows minimal adsorption of proteins, viruses, etc. Membrane retention is unaffected by repeated re-use. The Hydrosart® ultrafiltration membrane can be re-used without loss of integrity or performance.
Pore size|Retention rate
Hydrosart® ultrafiltration cassettes are available in a choice of the following nominal molecular weight cut offs:
10 kD|30 kD|100 kD
Filtration area
Sartocon® Slice 200 Cassette 200 cm2
Sartocon® Cassette 0.7 m2
Sartocon® Slice Cassette 0.14 m2
Sartocube® 3.5 m2 Cassette